This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14以太网Boot的问题

Other Parts Discussed in Thread: 66AK2H14

TI专家好,

我们打算做一块板子,板子上有4片66AK2H14,每片66AK2H14都不连接任何FLASH芯片(包括SPI FLASH或者NAND FLASH)。

而是将4片66AK2H14和1片FPGA连接到一个以太网SWITCH上,打算用FPGA通过以太网对66AK2H14进行BOOT。

1. 请问这种方式可行吗?

2. 通过什么工具,将DSP程序以及ARM Linux镜像转化为以太网包,从而发送给SOC,以BOOT SOC?

3.看processors.wiki.ti.com/.../KeystoneII_Boot_Examples HOST。如果用FPGA从网口BOOT,需要这些设置吗?FPGA直接将DSP程序加ARM Linux镜像按照指定格式,通过MAC帧发送给SOC,能BOOT SOC吗?