大家好:
想法:想用DM368的做一个并行双视频流,不知支持否?
从器件手册的管脚说明来看,其有如下描述,不知道是否就是我所理解的并行双视频流输入呢?
多谢。:)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM36x cannot take more than one video capture input.
Since pixel clock and even internal video pipeline is just one.
In DM36x-DVR, we used TVP5158 which could take 4CH D1 as input. The TVP5158 would then "line multiplex" the 4CHs so that it appears as one big frame to the DM36x. Then in DM36x in SW we would demultiplex this into individual frames. Refer to TVP5158 datasheet for details for this line multiplexed capture format.
The same line multiplexing in theory could be done by a FPGA for say 2x720p30.
However make sure the combined frame size and data rate is within the DM36x PCLK, line width limits.
理解: 1.AVID信号是用来裁剪视频的。 2.而FID是场信号,如果FID不是必须 的,那用来什么作用呢? 疑问: 1.那么DM368的C_WE_FIELD应该和什么管脚连接呢? 2.如图所示,我的设计是否可以呢? 谢谢
一般用BT656和BT1120这种内嵌同步的方式来传送视频的话, AVID和FID其实都有内嵌的字段来代替的,所以只需要连接PixelCLK 和 数据线即可。所以C_WE_FIELD不接也是OK的。
你好,
那我再理解一下。
1.疑问:是否意味着dm368是可以支持双路视频的?只不过要将两个视频输入的信号分别处理,例如当作一个big frame。
DM36x cannot take more than one video capture input.
Since pixel clock and even internal video pipeline is just one.
这两句和下面这句到底该如何理解呢?In DM36x-DVR....
如果将pclk分两路扇出是否可行?
我们现在就是准备这么设计,将PCLK分两路到两个视频解码芯片,然后一起接收过来。:)
每一路采用YCC8BIT。
譬如,我们可以采用两个tvp5151来分别对接到DM368的YCC输入接口上。
2.带来的另一个疑问是:当有两路视频输入时,是否这些WE_FIELD、AVID这些信号可以也不用管,因为BT协议中本身已经携带了同步信号、数据有效信号,那么只要在软件中创建两个视频捕获线程,分别捕获、分别过H.264就可以了?
3.这样的影响呢?是不是就是HDVICP的负荷就高了,譬如两路都是D1,那么他们的处理延时就是处理单路的两倍?
多谢。:)
1/2 DM368 的CAM口不支持两路8bit视频输入。 如果你打算在前端用个比如FPGA把两个D1拼成一个长或者宽达到D1两倍的这种接进来,再在芯片内部拆,是可行的,但是这个就不如直接采用TVP5158接入来的省事了。
3. DM368 可以压缩1080p30的H264,所以对于2路D1来说 , 是可以做实时的。 延时会比1路D1大,但是不会大很多。
你好,
我们的设计,其实是如下场景。
1.支持AV输入,一路。我们使用TVP5151支持AV编码到DM368,编码为YCC8BIT
2.支持HD输入,一路。使ADV7611支持HDMI编码到DM368,编码为YCC16BIT。
3.所以, 同时,DM368支持两个YCC8BIT,不知道理解对不?
所以,我们想在这种场景下,将两路视频都设置为YCC8BIT编码,通过DM368接收回来,然后作为两路视频处理。
疑问:就是第3个场景,不知能否实现?
在前面的回复里已经提到了,不支持两路8bit的视频同时接入。