您好!我想把DVSDK4.02环境下的tvp5146更换成tvp5151,请问我需要tvp5151的驱动代码吗?还是直接配置相应的寄存器?望指教!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

安装好了之后,里面找一下cmd格式的配置文件,文本格式打开,有例子的。
BR,
Eason
非常感谢您能回复!请问改寄存器配置的位置是在TVP514x.c文件里的tvp514x_write_regs的函数里面吗?除了修改寄存器配置还需要其他改动吗?望指教!
可以沿用原来的I2C配置函数,你注意下I2C地址是否存在不同就好了。
从tvp5146改到tvp5151, 你的用意是什么?如果都是接入CVBS并采用BT656的接口接入视频的话,是不需要再做改动了。