This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教C6678 DDR3 4GB使用问题!



现在使用的电路板上的6678挂4片DDR3,以前每片DDR3为4Gb,即一共为2GB,6678能正常访问DDR3。但是现在把4Gb颗粒升级为8Gb的颗粒(由两个4Gb叠加而成,有片选CS0,CS1信号,DDR3型号为MT41K512M16TNA125)发现访问有以下问题,麻烦知道的人能够给指点以下:

1.当不打开CS1,只开CS0的时候,即eBank设置为0的时候,6678能正常访问低2GB的存储空间

2.当想访问后2GB空间的时候,把eBank设置为1,同时设置XMPAXL1=0x880000BF,XMPAXH1=0x8000001E,发现这个时候DDR3的地址数据一直刷新,读写数据失败,同时XMPAXL1,XMPAXH1两个变量不设置,采用默认值访问前2GB,现象也是DDR3地址数据一直在刷新

总感觉用CS片选信号的时候,配置还有问题,但是确实找不到还有哪些相关的配置,麻烦知道的给指点下,多谢!