我在看资料“AM335x-PSP 04.06.00.03 Features and Performance Guide”时写着beaglebone支持uart0启动,但没有找到相关的资料具体说明如何启动,请问哪里有具体的启动指导?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我好像没有看到具体的指导,但你可以按照如下思路自己看看
1. 你看看TRM的 26章,找到sysboot的跳线方式,哪个是UART0启动的
2. 你看看bb的原理图,搜下SYS_BOOT15,然后找到syboot对应的跳线方式,跳号线
3. 在datasheet中可以找到UART0对应的pin 脚,然后在beaglebone上找到,可以发现uart0已经转成usb了,所以在pc上装好uart转usb的驱动
4,上电,在串口终端上可以看到C打印了,就是板子发bootme了,然后参考 processors.wiki.ti.com/.../AM335x_U-Boot_User%27s_Guide 就ok了
1. 传到板子上,uboot放到ddr里面,所以要先让spl工作
2. UART0通过一个uart 转 usb的片子,转到usb口了
3. TRM是针对AM335x片子的,和板子没关系,你可以看看http://beagleboard.org/
您好!请问您的uboot-spl.bin是是哪里找到的,我找了好久没有下载到。
跪谢!!!