This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14与K7的SRIO4x连接问题



各位好:

        如题,我目前把DSP作为从设备,程序设置为no_loopback,FPGA和SRIO之间的4个链路分别配置成1x模式、2.5Gbps,FPGA都能够从DSP端读写数据。但是一旦配置成SRIO4x模式,就会有如下错误:

[C66xx_0] SRIO test between two DSPs start............................................
Enable Exception handling...
SRIO path configuration 4xLaneABCD
Input port 0 next expected ackID value: 0x0
Output port 0 unacknowledged ackID: 0x0
Output port 0 next transmitted ackID value: 0x0
The output port 0 has encountered a degraded condition. The degraded port error threshold has been reached in the Port n Error Rate Threshold Register.
The output port 0 has encountered (and possibly recovered from) a transmission error. This bit is set when bit 16 is set.
The output port 0 is in the output error-stopped state.
The input port 0 has encountered (and possibly recovered from) a transmission error. This bit is set when bit 8 is set.
The input port 0 is in the input error-stopped state.
The input or output port 0 has encountered an error from which hardware was unable to recover.
Port 0 OK condition. The input and output ports are initialized, and the port is exchanging error-free control symbols with the attached device.
The port 0 detected a delineation error. The port received an unaligned /SC/ or /PD/ or undefined code-group. The capture registers do not have valid information during this error detection.
The port 0 experienced a link timeout. The port did not receive an acknowledge or link-response control symbol within the specified time-out interval. The capture registers do not have valid information during this error detection.
Type of information logged: 0 (0 - packet, 1 - control symbol)
captured error bit in the Port Error Detect Register: 31
control symbol or Bytes 0 to 3 of the packet header that correspond to the error: 0x0
Bytes 4 to 7 of the packet header that corresponds to the error: 0x0
Bytes 8 to 11 of the packet header that corresponds to the error: 0x0
Bytes 12 to 15 of the packet header that corresponds to the error: 0x0
15 8b/10b deconding error have occurred


SP[0]_ERR_STAT = 0x01010102
SP[0]_ERR_DET = 0x00000004
Corrected Error Stop Condition. SP[0]_ERR_STAT = 0x01010102

求教这是什么导致的?每个链路单独不都能够正常通信么?

  • 你好关于

    serdes ports 和lanes的关系不是特别清楚想请教你一下

    按照LANE和MODE的关系图

    例如采用2X MDOE1时即只有PORT0,PORT1工作,我可以理解是这连个PORT被当成一条LANE么?

    当我使用DIO传输的时候OUTPORTID怎么设置呢?

  • 你好:

            我理解lanes是指的物理链路,ports指的是逻辑上的接口,一个port可以包含多个lanes。mode1中的2X指的应该是一个包含两个链路(A和B)的port,而这个port的dest_id就看你要连接的另一个端点器件的ID设置了。

  • 哈哈非常感谢你的回答

    我理清楚了 4个port对应四条lanes,当设置成1x 1x时使用PORT 0,1

    但是当配置成2x,1x,1x时 使用的Port是0 ,2,3

    还有一个问题你改LOOPBACK模式时是将PORT SERDES都设置成了 LOOPBACK么

    我这样改的话总是卡在了 ISPORTOK部也就是 对应PORT STAT一直为0;

  • 借贵宝地一用。。

    请教楼主大侠一个问题

    用2个6678开发板互联SRIO, NWIRTE和NREAD命令后,DSP内存的中的数据读写都正确。

    但是在自制的项目中要求6678 和Xilinx ultrascale xcku040的SRIO互联时。调试中FPGA能接收来自DSP的NWRITE命令,并且将数据写入到RAM中。当DSP使用NREAD命令时,FPGA接收到了读指令,并且返回数据,但是绝大部分概率是DSP的内存没有更新,同时DSP提示“completion code =1”,偶尔会出现DSP的内存更新,同时DSP提示“completion code =0”。

         不是哪位大侠能分析下是什么原因导致的