请问 dvsdk4.02中的NANDWriter_DM36x.out 和dvsdk2.0中的NANDWriter_DM36x.out 有区别么,dm368平台可以用dvsdk2.0中的NANDWriter_DM36x.out 么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问 dvsdk4.02中的NANDWriter_DM36x.out 和dvsdk2.0中的NANDWriter_DM36x.out 有区别么,dm368平台可以用dvsdk2.0中的NANDWriter_DM36x.out 么?
可以说说为何关心这个的区别吗
源码可以在linux_lsp/xxxxlinux-pspxxxxx/host-tools/src下找到
手头没有这两个版本……
你好,是这样,我在dm368上移植dvsdk4.02,如果我移植ubl文件UBL_DM36x.bin,u-boot-2010.12,及linux-2.6.32.17内核在dm368上,运行encode编码264文件编码720p 60Hz,运行输出信息如下:
ARM Load: 26% Video fps: 30 fps Video bit rate: 1074kbps Sound bit rate: 0 kbp
s Time: 00:00:04 Demo: Encode Display: 720P 60Hz Video Codec: H.264 HP Resolutio
n: 1280x720 Sound Codec: N/A Sampling Freq: N/A
ARM Load: 28% Video fps: 30 fps Video bit rate: 1026kbps Sound bit rate: 0 kbp
s Time: 00:00:04 Demo: Encode Display: 720P 60Hz Video Codec: H.264 HP Resolutio
n: 1280x720 Sound Codec: N/A Sampling Freq: N/A
...........
如果我移植ubl文件UBL_DM36x_NAND_ARM432_DDR340_OSC24.bin,u-boot-2010.12,及linux-2.6.32.17内核在dm368上,运行encode编码264文件编码720p 60Hz,运行输出信息如下:
ARM Load: 20% Video fps: 22 fps Video bit rate: 980kbps Sound bit rate: 0 kbp
s Time: 00:00:04 Demo: Encode Display: 720P 60Hz Video Codec: H.264 HP Resolutio
n: 1280x720 Sound Codec: N/A Sampling Freq: N/A
ARM Load: 19% Video fps: 22 fps Video bit rate: 760kbps Sound bit rate: 0 kbp
s Time: 00:00:04 Demo: Encode Display: 720P 60Hz Video Codec: H.264 HP Resolutio
n: 1280x720 Sound Codec: N/A Sampling Freq: N/A
.............
以上除了烧写ubl文件的不同以外,其它的都一样,但encode编码出的文件确差别较大,烧写了UBL_DM36x.bin这个文件,编码出的264文件可以正常播放;而烧写了UBL_DM36x_NAND_ARM432_DDR340_OSC24.bin文件,编码后播放该264文件不正常,有丢帧,视频播放也快。请问这是什么原因呢?是时钟的区别还是有其它问题?谢谢.....