This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于8168scalar模块求教



整个系统是这样的:2路dvi输出到两个显示屏,使用了2个mosaic,每个mosaic都有一个scalar,按设计原始计划是一个显示屏只能显示3个1080p20,但是我现在确可以在一个显示屏显示6个高清,但是另一个屏就一个都不能输出。这不是很奇怪么,按理说一个屏的scalar只能处理170MP/s的码流呀

SwMsLink_CreateParams       swMsPrm[VDIS_DEV_MAX];// VDIS_DEV_MAX 4

swMsPrm[0].swMsInstId[0] = SYSTEM_SW_MS_SC_INST_DEI_SC_NO_DEI;//SYSTEM_SW_MS_SC_INST_DEI_SC_NO_DEI;
swMsPrm[0].swMsInstId[1] = SYSTEM_SW_MS_SC_INST_VIP1_SC;

swMsPrm[1].swMsInstId[0] = SYSTEM_SW_MS_SC_INST_DEIHQ_SC_NO_DEI;//SYSTEM_SW_MS_SC_INST_DEIHQ_SC_NO_DEI;
swMsPrm[1].swMsInstId[1] = SYSTEM

6个1080p显示在一个屏上,很正常,按理说,两个mosaic处理的应该没有z序的概念,但是,从我显示的情况看,z序也是正常的,这个怎么解释,迷茫中,求指导,谢谢!!!

6个视频窗口不管是开6方格,还是叠加,都一样。

还有一个,就是,按8168hdvpss中所说,如果d1的信号开在1080p的窗口,是按1080p去计算资源的,可是,为什么我开d1的,分辨率接近1080p,却能开10个以上,求解释!

  • 你好,

    一个scaler硬件的性能是和HDVPSS配置的频率成正比的,一般你可以用HDVPSS的频率乘以70%~80%作为SC处理性能的理论值。所以如果你使用的DM8168的HDVPSS支持的频率大于200Mhz,那SC的处理能力是比170MP/s强。

    你说你可以输入6个1080p,请问你确认你的帧率可以达到每路20帧么?你可以检查一下处理时间。

    什么叫开D1的?是输入SWMS的图像是D1,让后拼接为一个1080p的输出么?