This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

能通过DM8168的Vout0和SPI接口设计一个4.3寸或者7寸LCD触摸屏接口吗?



最近要做一个采集两路VGA进行264编码存到硬盘,再进行264解码输出两路VGA信号的产品,还得再加一个LCD触摸显示屏,用于浏览文件,所以想咨询下,能用扩展的Vout0和SPI实现不?感觉理论上应该是可行的,但是之前没有接触过DSP这块,所以想跟各位DSP工程师们想求证下,谢谢~

另外咱们有这样的相应的参考设计资料吗?非常感谢~

刚才发的一个帖子,不知道为什么要通过版主审核才能显示,可能是有些关键字不符合吧,比较着急,所以又发了一个,版主帮我把之前那个需要审核的删了吧,谢谢~