在C6678的评估板中,采用了UCD9222和UCD7242给DSP提供CVDD和CVDD1;而在评估板上的FPGA,则控制上电后CVDD和CVDD1的上电顺序。
我想问的是,如果我自己做板子,是不是首先要使用“Fusion Digital Power Designer”软件对UCD9222配置,然后FPGA的控制才有效?
如果是,那么我是不是还需要购买一根TI USB adapter连接PMbus?如果需要,这个在哪里购买?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
yangkang yangkang,您好
使用Fusion Digital Power Designer配置UCD9222,就可以随意控制CVDD和CVDD1的上电时序和延时。
如果要使用电脑在Fusion Digital Power Designer上配置UCD9222,需要买一个“USB-TO-GPIO - USB Interface Adapter EVM”,可以在以下网站购买:
https://estore.ti.com/USB-TO-GPIO-USB-Interface-Adapter-EVM-P960.aspx
如果自己做板子,要将UCD9222的PMBus引脚引出来,以匹配“USB-TO-GPIO - USB Interface Adapter EVM”。
“USB-TO-GPIO - USB Interface Adapter EVM”的接口描述详见
http://www.ti.com/tool/usb-to-gpio
上的文档“USB Interface Adapter Evaluation Module”的第30页。
谢谢
Kevin Zhang,
很感谢你的回答!看来那根线是可以不用买的,我现在想通过FPGA控制UCD9222。
在C6678 评估板中,UCD9222的PMBus是出来和FPGA相接的;而且我下载了evm板中fpga的代码,下载地址为:www.advantech.com/.../6678le_download3.aspx。
fpga中对PMBus的操作并不是很多,主要就是控制CVDD和CVDD1先后使能,进而实现CVDD和CVDD1不同时间给C6678供电。
我下载的FPGA代码不知道是否是完整的,是否是烧写在板子上的FPGA内的比特文件所对应的源代码。如果是,我想问的是,难道不需要设置CVDD和CVDD1的电压值么?