This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM368的ARM926内核寄存器的物理地址



ARM9内核是有37个寄存器,R0、R1……CPSR等,这些寄存器是否在DM368 4G的寻址空间中?它们对应的物理地址是什么?在ARM RAM0 Instruction(0x0000 0000~0x0000 3FFFF),ARM RAM1 Instruction(0x0000 4000~0x0000 7FFFF),还是ARM RAM0 Data(0x0001 0000~0x0001 3FFFF),ARM RAM1 Data(0x0001 4000~0x0001 7FFFF)?谢谢!

  • 你需要做什么用途?调试的话,请用CCS挂仿真器去看这些寄存器的值

  • Eason你好,我需要做一些研究方面的工作。XDS560 V2仿真器配合CCS6.0的方法我做用过,刷新时间最短只能设置为0.1s,而且我也未能找到自动保存的设置。现在用的是J-Link仿真器,通过命令行的方式读取寄存器的值。J-Link命令行可以将某个或某段地址的值保存为bin文件,但不能按寄存器名保存,所以我想确定寄存器的物理地址。谢谢!