This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM8168的SWMS模块的性能及并发问题



swms模块配置如下: swMsPrm[i].numSwMsInst = 4; swMsPrm[i].swMsInstId[0] = SYSTEM_SW_MS_SC_INST_SC5 ; swMsPrm[i].swMsInstStartWin[0] = 0; swMsPrm[i].swMsInstId[1] = SYSTEM_SW_MS_SC_INST_VIP1_SC; swMsPrm[i].swMsInstStartWin[1] = 4; swMsPrm[i].swMsInstId[2] = SYSTEM_SW_MS_SC_INST_DEIHQ_SC_NO_DEI ; swMsPrm[i].swMsInstStartWin[2] = 6; swMsPrm[i].swMsInstId[3] = SYSTEM_SW_MS_SC_INST_DEI_SC_NO_DEI; swMsPrm[i].swMsInstStartWin[3] = 8; 共用了4个模块,每个模块负责2路多画面处理,问题如下: 1、4个模块同时使用,如果两个模块的目标画面区域有交集,会否出现互相覆盖闪烁的问题,及PIP的形式会出现重叠区域闪烁; 2、这4个模块的多画面scaler性能有没有差异,哪个会是最强 3、单独来看SYSTEM_SW_MS_SC_INST_SC5这个模块最多能够同时进行多少路1080P60源画面的scaler 4、如果同样大小的目标,源采用CROP和不采用CROP对性能有没有影响

  • 你好,

    1. 请问你使用的软件是否是最新的DVR RDK4.01软件?

    2. 每个SC的性能相当。

    3. 请参考讨论:http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/p/90405/232109.aspx#232109。

    4. 对于SC性能的消耗,看输入/输出SC较大的那个分辨率。

  • 其中还包含一个重要的问题分支,就是如果4个同时使用,每个swms处理2路共8路,即inst1处理id0-1,inst2处理id2-3,inst3处理id4-5,inst4处理id6-7;

    能否保证id越大,图层越在上面,能够有效覆盖下层的图像,即图层自上而下id7,6,5,4,3,2,1,0,但实测下来发现上下图层如果不在同一个inst中,则相交叉的区域会出现闪烁问题,有没有解决办法。谢谢!