Dear engineers
我在进行6638 PCB设计过程中遇到如下难题,麻烦大神给予不吝赐教,多谢!!
1. 在Hardware Design user guide中看到这段话“In the event a partial number of lanes are used (two lanes instead of four), all clock and data pins must be connected. Unused lanes (both transmit and receive) can be left floating”。
问题:确认一下是否可以只连接2条lane(即只连接2条lane的差分收发),其他2条悬空,如果可以,该怎样选择哪两条?
2. Hyperlink速度较高参照SerDes Implementation Guidelines for KeyStone I Devices给出的约束进行,其中提到:" HyperLink lanes can be swapped to simplify routing. The differential pairing must be maintained",请问Layout过程中的每4对差分收发是真的可以交换吗?如果交换以后程序中的那个寄存器可以重新设置差分对的通道号?