This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM388非常热,温度达80摄氏度,另外系统无规律死机,求思路,想法,方案

Other Parts Discussed in Thread: TVP5158

    公司正使用DM388开发IPC,CPU以600Mhz、DDR:533Mhz运行时,相机框体表面温度高达65-70摄氏度,内部金属结构75-80摄氏度,我是一个纯软件人员,硬件方面不大了解。公司的硬件工程师我看来是个奇葩,解决问题的思路异想天开,加散热片,换铝制外壳,加风扇,等等等等,就差用液冷了,虽然有一定作用,但加风扇之类的思路明显不可取。因为系统常常跑几天就死机,而引起死机的原因却又无法查明,软硬件工程师互相推诿,影响工作气氛和进度,为此,我提出以下问题

1.系统硬件方面

    电源管理:我司的IPC最大功耗经测试高达7W. 海思的一个类比方案只有2W. 

    TI的电源管理:www.ti.com/.../TIDA-00079 此处的说3W~4W左右的功耗就可以实现最大性能

    因此,我严重怀疑我司硬件工程师的电源管理,故请问:DM388方案的最大功耗是多少?硬件上如何改善功耗?我司并没有采用上面TI的解决方案。

2.系统软件方面

    编译时使用低功耗模式,单码流,分辨率降低到720P, 关闭3D降噪、WDR等等,都没有明显改善,使用Top命令查看CPU占有百分比,并没有什么进程高占用率。请问还有什么地方需要优化?

3.如果不是过热引起的系统过几天就无规律的死机,那么如何诊断和解决?

期盼您的各种想法和思路,谢谢!