This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am3358镜像烧写问题

Other Parts Discussed in Thread: AM3358, FLASHTOOL

各位工程师:

       你们好,我用Uniflash3.0通过USB进行eMMC的烧写,板子电源管理,cpu,eMMC以及DDR都和bbblack相同,SDK是Android 4.2.2, SYSBOOT pin选择的是:MMC1 MMC0 UART0 USB0。

我在网上买了一个USB to TTL的板子接到了am3358的uart0上,用来看烧写时的log信息,用AM3358的USB0来烧写镜像。flasher image用的是论坛上BBBlack的,

依照烧写文档对第一次新出现的网络进行了配置,但是点start flashing后,进度一直未0%,且am3358上电后,uart0端没有输出“CCCCC”

在Uniflash3.0的安装目录中看opentftp.log信息,如下:

[27-Jul-15 09:45:41] Open TFTP Server MultiThreaded Version 1.64 Windows Built 2001 Starting..
[27-Jul-15 09:45:41] starting TFTP service
[27-Jul-15 09:45:41] alias / is mapped to C:\AM335x_Flashtool\images\
[27-Jul-15 09:45:41] permitted clients: all
[27-Jul-15 09:45:41] server port range: all
[27-Jul-15 09:45:41] max blksize: 65464
[27-Jul-15 09:45:41] default blksize: 512
[27-Jul-15 09:45:41] default timeout: 3
[27-Jul-15 09:45:41] file read allowed: Yes
[27-Jul-15 09:45:41] file create allowed: No
[27-Jul-15 09:45:41] file overwrite allowed: No
[27-Jul-15 09:45:41] thread pool size: 1
[27-Jul-15 09:45:41] Listening On: 192.168.2.1:69
[27-Jul-15 09:45:57] Client 192.168.2.3:1234 C:\AM335x_Flashtool\images\u-boot-spl-restore.bin, 200 Blocks Served

到这里就没了,opendhcp.log如附件, 看tftp的log,感觉u-boot-spl-restore.bin已经烧写成功了,那么后面没烧写是因为什么呢?请各位帮忙解答一下,谢谢。