tms310dm8148的ISS模块的具体说明资料找不到,现今需要知道ISS模块最高支持多少像素,以及相应的帧率
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
通过CAM口和CSI口均可接入1080p60。
pixel的throughput大致可以按照这个值为准估算。
4K也可以接入,帧率约为15fps。
可以参考一个现有的参考设计:
http://appropho.com/NewWeb/Product_DM388IMX172.php
DM38x和DM8127的ISS部分大致是一样的。
BR,
Eason
但是dm388参考设计中并没有给出具体的帧率参考,一般芯片的具体sensor接口的pixel rate都应该会比编解码的速率要更高一点
另外,8148的datasheet中有这样一段 Image Sensor Interface (ISIF) features:
– Support for up to 32K pixels (image size) in both the horizontal and vertical direction,
是说明ISS接口最高能支持32K X 32K =1024M,接口分辨率吗?