This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

板子无法connect!!



大家好!

昨天跑程序的时候一直正常的,跑的过程中突然console打印了一堆红色字的信息然后所有核就disconnect了,当时没在意,我就下电放了一会然后重连,但是就连不上了。现在还是连不上。。

在ccxml中test connect显示:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

F:\ti\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.

An already open status was returned while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-110' (0xffffff92).
The title is 'SC_ERR_OCS_ALREADY_OPEN'.

The explanation is:
This utility opened the controller but found it already in use.
You must exit other debuggers and utilities that access the
controller because this utility must be the only client.

[End]

lanch可以,但connect的时候显示:

Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.507.0)

我的板子是TMDSEVM6678L,主板上面不带那块小的仿真器,connection选的是Texas Instruments XDS100v1 USB Emulator.

怎么解决????

谢谢!