8148平台,硬件把5158更换为5150,软件中需要修改那些文件?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TVP5150是单路Video Decoder, TVP5158是多路的。
在DVRRDK中,你需要修改capturelink中的相关参数,改为单路采集。在你的usecase中,多路的部分也会需要做相应的修改。
TVP5150本身要工作起来,也需要配置几个I2C寄存器,这个部分需要你自己加。
BR,
Eason
hi Eason
谢谢你的回复,可以具体详细点吗,关于capturelink中的相关参数和usecase中,我主要修改了原来的4通道为现在的1通道(原来的5158,我们也只用了一个通道采集),关于5150的i2c配置,我是在5158的基础上修改的,只配置了03寄存器,其他的没有配置,启动程序后没有图像,如果想正常工作,我们具体需要配置那些必须的寄存器。
这个问题早解决了,你的回答还是有帮助的,5150有个PDN没有设置好造成