开发环境:DM385, IPNC3.5
DM385的uboot启动的时候,MLO正常的加载启动后,可以读到u-boot.bin,为什么u-boot没有运行呢 ???
U-Boot 2010.06-dirty (Aug 09 2015 - 11:22:11) DM385_IPNC_3.50.00
DM385-GP rev 1.1
ARM clk: 600MHz DDR clk: 533MHz L3 clk: 200MHz IVA clk: 450MHz ISS clk: 400MHz DSP Default OFF DSS Default OFF
DRAM: 1 GiB MMC: OMAP SD/MMC: 0, ON-BOARD SDIO: 1 Using default environment
The 2nd stage U-Boot will now be auto-loaded Please do not interrupt the countdown till DM385_IPNC prompt if 2nd stage is already flashed Hit any key to stop autoboot: 0 reading u-boot.bin
204364 bytes read ## Starting application at 0x80800000 ...
请大家帮忙分析一下,谢谢;