This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 EVM 板和PC机通过网口通信的问题



我想实现6678的EVM板和PC机通过网口传输数据,在ti/mcsdk_2_00_05_17/examples/ndk/client有工程client,我改了client.c中的几个地方:

line 81    *LocalIPAddr 改为 192.168.1.122;

line 83    *GatewayIP   改为192.168.1.1;

line  90    clientMACAddress  改为我电脑的MAC地址.

编译运行此工程,Console窗口中打印出信息:

QMSS successfully initialized

CPPI successfully initialized

 PA successfully initialized

 Tcp/IP stack Example client

configuring DHCP client

PASS successfully initialized

Ethernet eventId  :  48  and  VectId (Interrupt)  :  7

Registration of the EMAC successful ,waiting for link up...

Service status   :  DHCPC  :     Enabled  :                   : 000

Service status   :  Telnet  :       Enabled  :                   : 000

Service status   :  HTTP  :        Enabled  :                   : 000

Service status   :  DHCPC  :   Enabled  :   running   : 000

Service status   :  DHCPC  :   Enabled  :   Fault        : 002

Service status   :  DHCPC  :   Disabled:                   : 000

打开PC机的CMD窗口,输入"ping 192.168.1.122",cmd窗口显示信息如下:

 Pinging 192.168.1.122 with 32 bytes of data:

Request timed out

Request timed out

Request timed out

Request timed out

Ping statistics for 192.168.1.122

packets : Sent = 4,  Received = 0 ,  Lost = 4(100% loss).

         我对NDK的代码不懂,可有哪位网友知道为什么连接不上吗?是不是我缺少什么步骤还是哪个地方的代码还需要改?希望各位高手不吝赐教。

2.    现在我自己的板子上有两片6678的DSP,我想在这两个DSP之间通过网口传输数据,但是一点头绪都没有,不知道该怎么办,可有哪位高手知道具体的步骤吗?

        希望得到大家的帮助,十分感激!

        祝大家一切顺利!

        Nuoxi