This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 PLLC1SYSCLK6或PLLC2SYSCLK5 内部时钟配置

Expert 1222 points


Hi,

目前使用的是DM368 需要接入TFT 800*480 LCD, 但是需要让DM368 VCLK/GPIO79 引脚输出30MHZ- 50MHZ 时钟频率以提供给LCD pclk .

需要配置PLLC1SYSCLK6 或PLLC2SYSCLK5 让其输出需要的时钟..(其他外部时钟硬件均为接入)

请问怎么配置?

  • 你好,

    当VCLK输出大于27Mhz的时候,需要外部输入时钟到DM36x来作为VCLK的输入源。

    下面的信息可以在数据手册里面找到:

    GIO80 / EXTCLK /B2 / PWM3 /PWM3/  B19

    Input GIO: GIO[80]
    Video Encoder: External clock Input, used if clock
    rates > 27 MHz are needed, e.g. 74.25 MHz for
    HDTV digital output.