This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x cpsw问题



如图,现在使用一个交换机芯片和am335x相连,本来的交换功能正常,就是四个口都已经相通了,但是ping的功能不正常,修改cpsw_slaves[]中的字段.phy_id = "0:00", 这样可以Ping通第一个口,绿色线走向,修改cpsw_slaves[]中的字段.phy_id = "0:01",可以ping 通第二个口,黄色线走向,
这个交换机芯片以前用到其他的soc上,都可以正常使用ping通各个口的,所以我现在怀疑这个cpsw驱动的问题
请问有哪些资料可以指导修改的吗,或者例子链接之类的,谢谢