This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657不能使能PLL mode 报错 Encountered Illegal Op-code



大家好

我的板子可以通过ccxml的“test connection”测试,jtag可以连接到器件。
执行KeyStone_main_PLL_init(100, 10, 1)最后一步:

gpPLLC_regs->PLLCTL |= CSL_PLLC_PLLCTL_PLLEN_MASK;/*14. Set the PLLEN bit in PLLCTL to 1 to enable PLL mode*/

提示如下:
C66xx_0: Encountered Illegal Op-code
C66xx_1: Encountered Illegal Op-code
C66xx_1: Trouble Reading Register PC: (Error -1178 @ 0x6E) Device functional clock appears to be off. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)

如果屏蔽掉不执行 gpPLLC_regs->PLLCTL |= CSL_PLLC_PLLCTL_PLLEN_MASK,则没有错误提示 也可以进行后续操作。我是通过晶振输出100M直接给的6657,DSPPLL mode不使能,,这时 6657的核时钟也就是100M,难道这个6657不能倍频到1G???

如此 是我的晶振信号有问题 还是6657芯片有问题,还是电源有问题???(我的另外一块板子没有遇到这个问题)

求各位朋友解答!!!谢谢!