This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100V3不能检测到AM3352 问题

Other Parts Discussed in Thread: AM3352

新板打样归来,用XDS100V3仿真AM3352,不能检测到内核

检测过JTAG接口连接,启动方式,晶体振荡没发现大问题,电源芯片电压测试如下:

VDD1_SMPS:1.109V
VDD2_SMPS:1.095V
VDDS_DDR:1.5V

VDIG2:1.8V
VAUX1:1.8V
VDAC:1.81V

VAUX33:3.3V
VMMC:3.3V
VAUX2:3.3V

CCS安装完后,选择芯片型号和仿真器类型,点击TEST CONNECTION显示错误如下,请问是什么原因,谢谢。

 
An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.