This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C674x DSP L1 L2 及cache设置



目前从事DM8148平台的开发工作,想请教一个问题:

通常情况下,数据从外存通过EDMA搬移到L2 cache,然后L1 cache 命中,供CPU访问,CPU处理完数据,在通过EDMA 将处理完成数据从L1 cache,L2 cache,搬到指定的外存。

如果直接将数据从外存通过EDMA搬移到L1 SRAM,然后CPU处理,处理完成的数据直接从L1 SRAM通过EDMA传到外存指定空间,这样操作可以?做了个小实验是可以的。

但是这样数据流操作就和L2 ,L1 chache没有任何关系了?

这样的数据流和数据流“外存-->L2-->L1-->CPU-->L1-->L2-->外存”方式有什么样的差别?

也就是说这两种方式之间的性能优劣,及对L1 和L2 cache及SRAM 的影响?

请大侠帮忙,谢先!