This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x 3.3V电压升高



手里一个板子用的am335x,电源管理芯片是TPS65217C,板子分为核心板和底板,核心板上主要由CPU、电源管理、Flash、DDR组成,底板上有一个RS485接口,现在有个问题是,当底板上焊接MAX13487芯片时,核心板上am335x的3.3V电压会被拉升到4.3V左右,如果断开MAX13487的RXD引脚,则核心板3.3V电压正常,MAX13487是5V供电,且RXD经10K电阻上拉到5V。各位有没有遇到过类似的问题,可能是什么原因呢

我试过去掉RXD的上拉电阻,但是核心板3.3V电压还是4.3V,我量过坏的板子上485对应的RXD引脚电压是4.9V,好的板子上RXD引脚对应的电压是4.1V。测量坏的板子RXD与5V之间阻抗与好的板子是一样的,都是7MΩ左右。