This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl138 从NAND启动,uboot加载linux 内核报 bad data crc错



使用2015年4月份的u-boot,使用创龙核心板加自制的底板,总线上挂接16C554串口芯片,出现从nand启动后u-boot加载linux内核时报 bad datacrc错误,在U-BOOT中reset后可以正常加载内核,创龙核心板使用的是 spansion 型号为S34ML04G2 的512M flash,。

Loading from nand0, offset 0x120000
   Image Name:   Linux-3.3.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2843400 Bytes = 2.7 MiB
   Load Address: c0008000
   Entry Point:  c0008000
## Booting kernel from Legacy Image at c0700000 ...
   Image Name:   Linux-3.3.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2843400 Bytes = 2.7 MiB
   Load Address: c0008000
   Entry Point:  c0008000
   Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!