This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RDK8127,DSP模块无调试信息输出是怎么回事?

Other Parts Discussed in Thread: TPS65910

我也遇到了那个“TimeOut occure in boot_proc.Program exit.”的问题,不过,通过对比我的启动日志和网上别的RDK8127的日志,发现我的启动过程中缺少了很多个[c6xdsp ]开头的调试信息输出。请教一下可能的原因会是什么?

  • 部分启动日志:

    NR_IRQS:375
    IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    Total of 128 interrupts on 1 active controller
    GPMC revision 6.0
    Trying to install interrupt handler for IRQ368
    Trying to install interrupt handler for IRQ369
    Trying to install interrupt handler for IRQ370
    Trying to install interrupt handler for IRQ371
    Trying to install interrupt handler for IRQ372
    Trying to install interrupt handler for IRQ373
    Trying to install interrupt handler for IRQ374
    Trying to install type control for IRQ375
    Trying to set irq flags for IRQ375
    OMAP clockevent source: GPTIMER1 at 20000000 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 598.01 BogoMIPS (lpj=2990080)
    pid_max: default: 32768 minimum: 301
    Security Framework initialized
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    devtmpfs: initialized
    omap_voltage_early_init: voltage driver support not added
    regulator: core version 0.5
    regulator: dummy:
    NET: Registered protocol family 16
    omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
    omap_voltage_add_dev: VDD specified does not exist!
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    omap_mux_init: Add partition: #1: core, flags: 4
    _omap_mux_init_gpio: Could not set gpio79
    _omap_mux_init_gpio: Could not set gpio80
    Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
    registered ti81xx_vpss device
    registered ti81xx_vidout device
    registered ti81xx on-chip HDMI device
    registered ti81xx_fb device
    PWM0 init success.
    PWM1 init success.
    bio: create slab <bio-0> at 0
    SCSI subsystem initialized
    USBSS revision 4ea2080b
    registerd cppi-dma Intr @ IRQ 17
    Cppi41 Init Done
    omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
    regulator: VRTC: 1800 mV
    regulator: VIO: 1500 mV
    regulator: VDD1: 600 <--> 1500 mV at 1100 mV
    regulator: VDD2: 600 <--> 1500 mV at 1350 mV
    regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV
    regulator: LDO1: 1100 <--> 3300 mV at 1800 mV
    regulator: LDO2: 1100 <--> 3300 mV at 1800 mV
    regulator: LDO3: 1100 <--> 3300 mV at 3300 mV
    regulator: LDO4: 1100 <--> 3300 mV at 1800 mV
    regulator: LDO5: 1100 <--> 3300 mV at 3300 mV
    regulator: LDO6: 1100 <--> 3300 mV at 3300 mV
    regulator: LDO7: 1100 <--> 3300 mV at 3300 mV
    regulator: LDO8: 1100 <--> 3300 mV at 1800 mV
    tps65911-rtc tps65911-rtc: rtc core: registered tps65911-rtc as rtc0
    tps65910 1-002d: No interrupt support, no core IRQ
    Advanced Linux Sound Architecture Driver Version 1.0.23.
    Switching to clocksource gp timer
    musb-hdrc: version 6.0, peripheral, debug=0
    musb-hdrc musb-hdrc.0: dma type: dma-cppi41
    MUSB controller-0 revision 4ea20800
    musb-hdrc musb-hdrc.0: USB Peripheral mode controller at c581e000 using DMA, IRQ 18
    NET: Registered protocol family 2
    IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
    TCP established hash table entries: 4096 (order: 3, 32768 bytes)
    TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    NetWinder Floating Point Emulator V0.97 (double precision)
    PMU: registered new PMU device of type 0
    omap-iommu omap-iommu.0: ducati registered
    omap-iommu omap-iommu.1: sys registered
    JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    msgmni has been set to 140
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    CMEMK module: built on Aug  5 2015 at 11:17:33
      Reference Linux version 2.6.37
      File /home/swxx/ti/Source/ti_tools/linuxutils_3_22_00_02/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
    allocated heap buffer 0xc7000000 of size 0x4000000
    cmemk initialized
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
    console [ttyO0] enabled, bootconsole disabled
    console [ttyO0] enabled, bootconsole disabled
    omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
    omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
    omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
    brd: module loaded
    loop: module loaded
    omap2-nand driver initializing
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
    Creating 7 MTD partitions on "omap2-nand.0":
    0x000000000000-0x000000020000 : "U-Boot-min"
    0x000000020000-0x000000260000 : "U-Boot"
    0x000000260000-0x000000280000 : "U-Boot Env"
    0x000000280000-0x0000006c0000 : "Kernel"
    0x0000006c0000-0x00000c000000 : "File System"
    0x00000c000000-0x00000cc00000 : "Data"
    0x00000cc00000-0x000010000000 : "Reserved"
    davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    davinci_mdio davinci_mdio.0: detected phy mask fffffffe
    davinci_mdio.0: probed
    davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
    mice: PS/2 mouse device common for all mice
    i2c /dev entries driver
    Linux video capture interface: v2.00
    OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
    notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbfd00000
    asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
    asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
    ALSA device list:
      #0: TI8148 IPNC
    TCP cubic registered
    NET: Registered protocol family 17
    Registering the dns_resolver key type
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    omap_voltage_late_init: Voltage driver support not added
    Power Management for TI81XX.
    Detected MACID=0:e0:a:dd:0:0
    tps65911-rtc tps65911-rtc: setting system clock to 2011-03-17 10:56:51 UTC (1300359411)
    mmc0: new high speed SDHC card at address 59b4
    mmcblk0: mmc0:59b4 00000 14.9 GiB
     mmcblk0: p1 p2

    CPSW phy found : id is : 0x4dd074
    PHY 0:01 not found
    IP-Config: Complete:
         device=eth0, addr=192.168.1.2, mask=255.255.255.0, gw=192.168.1.1,
         host=RDK_SWXX, domain=, nis-domain=(none),
         bootserver=192.168.1.1, rootserver=192.168.1.1, rootpath=
    Waiting 5sec before mounting root device...
    PHY: 0:00 - Link is Up - 100/Full
    VFS: Mounted root (nfs filesystem) on device 0:14.
    devtmpfs: mounted
    Freeing init memory: 192K
    INIT: version 2.86 booting
    Please wait: booting...
    Error opening /dev/fb0: No such file or directory
    Starting udev
    udevd (77): /proc/77/oom_adj is deprecated, please use /proc/77/oom_score_adj instead.
    udev: starting version 141
    udevd-event[80]: error changing netif name eth0 to eth8: Device or resource busy

    Root filesystem already rw, not remounting
    Caching udev devnodes
    Populating dev cache
    NOT configuring network interfaces: / is an NFS mount
    rm: cannot remove '/tmp': Device or resource busy
     inside finish.sh
    numid=1,iface=MIXER,name='PCM Playback Volume'
      ; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
      : values=127,127
      | dBscale-min=-63.50dB,step=0.50dB,mute=0
     [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
     [m3video] Remote Debug Shared Memory @ 0xbff05020
     [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
    SysLink version : 2.10.06.28
    SysLink module created on Date:Aug  5 2015 Time:11:23:13
    Trace enabled
    Trace SetFailureReason enabled
    /dev/mem opened.
    data 2
                 BW Phy Addr : 0x48180d00 Data : 0x00030000
                 AW Phy Addr : 0x48180d00 Data : 0x00030002
    data 3
                 BW Phy Addr : 0x48180d10 Data : 0x00000007
                 AW Phy Addr : 0x48180d10 Data : 0x00000003
    data 2
                 BW Phy Addr : 0x48180700 Data : 0x00000001
                 AW Phy Addr : 0x48180700 Data : 0x00000002
    data 2
                 BW Phy Addr : 0x48180720 Data : 0x00070000
                 AW Phy Addr : 0x48180720 Data : 0x00070002
    data 2
                 BW Phy Addr : 0x48180724 Data : 0x00030000
                 AW Phy Addr : 0x48180724 Data : 0x00000002
    data 60020
                 BW Phy Addr : 0x48140924 Data : 0x000e0020
                 AW Phy Addr : 0x48140924 Data : 0x000e0020
    data 60020
                 BW Phy Addr : 0x48140928 Data : 0x000c0040
                 AW Phy Addr : 0x48140928 Data : 0x000c0040
    data 60001
                 BW Phy Addr : 0x48140c18 Data : 0x000e0001
                 AW Phy Addr : 0x48140c18 Data : 0x000e0001
    data 60001
                 BW Phy Addr : 0x48140c1c Data : 0x000e0001
                 AW Phy Addr : 0x48140c1c Data : 0x000e0001
    data 2
                 BW Phy Addr : 0x48181564 Data : 0x00000002
                 AW Phy Addr : 0x48181564 Data : 0x00000002
    data 2
                 BW Phy Addr : 0x48181568 Data : 0x00030000
                 AW Phy Addr : 0x48181568 Data : 0x00000002
                 Phy Addr : 0x48181560 Data : 0x00000002
    data 2
                 BW Phy Addr : 0x48181560 Data : 0x00000002
                 AW Phy Addr : 0x48181560 Data : 0x00000002
    data 60002
                 BW Phy Addr : 0x48140aac Data : 0x00040002
                 AW Phy Addr : 0x48140aac Data : 0x00040002
    data 60002
                 BW Phy Addr : 0x48140ab0 Data : 0x00060002
                 AW Phy Addr : 0x48140ab0 Data : 0x00060002
    data 60002
                 BW Phy Addr : 0x48140ab8 Data : 0x00040002
                 AW Phy Addr : 0x48140ab8 Data : 0x00040002
    data 60020
                 BW Phy Addr : 0x48140a58 Data : 0x000c0080
                 AW Phy Addr : 0x48140a58 Data : 0x000c0080
    data 60080
                 BW Phy Addr : 0x48140a60 Data : 0x000c0080
                 AW Phy Addr : 0x48140a60 Data : 0x000c0080
    data 60020
                 BW Phy Addr : 0x48140a64 Data : 0x000c0080
                 AW Phy Addr : 0x48140a64 Data : 0x000c0080
    data 60020
                 BW Phy Addr : 0x48140a68 Data : 0x000c0080
                 AW Phy Addr : 0x48140a68 Data : 0x000c0080
    data 60002
                 BW Phy Addr : 0x48140aa8 Data : 0x00040002
                 AW Phy Addr : 0x48140aa8 Data : 0x00040002
    data 60002
                 BW Phy Addr : 0x48140aa4 Data : 0x00040002
                 AW Phy Addr : 0x48140aa4 Data : 0x00040002
    data 60002
                 BW Phy Addr : 0x48140aa0 Data : 0x00040002
                 AW Phy Addr : 0x48140aa0 Data : 0x00040002
    data 60002
                 BW Phy Addr : 0x48140a9c Data : 0x00060002
                 AW Phy Addr : 0x48140a9c Data : 0x00060002
    data 60002
                 BW Phy Addr : 0x48140a98 Data : 0x00060002
                 AW Phy Addr : 0x48140a98 Data : 0x00060002
    data 60002
                 BW Phy Addr : 0x48140a94 Data : 0x00060002
                 AW Phy Addr : 0x48140a94 Data : 0x00060002
    data 60002
                 BW Phy Addr : 0x48140a90 Data : 0x00060002
                 AW Phy Addr : 0x48140a90 Data : 0x00060002
    data 60002
                 BW Phy Addr : 0x48140a8c Data : 0x00060002
                 AW Phy Addr : 0x48140a8c Data : 0x00060002
    data 60002
                 BW Phy Addr : 0x48140a6c Data : 0x000e0002
                 AW Phy Addr : 0x48140a6c Data : 0x000e0002
    data 60002
                 BW Phy Addr : 0x48140a70 Data : 0x000c0002
                 AW Phy Addr : 0x48140a70 Data : 0x000c0002
    data 60002
                 BW Phy Addr : 0x48140a74 Data : 0x000e0002
                 AW Phy Addr : 0x48140a74 Data : 0x000e0002
    data 60002
                 BW Phy Addr : 0x48140a78 Data : 0x000e0002
                 AW Phy Addr : 0x48140a78 Data : 0x000e0002
    data 0
                 BW Phy Addr : 0x411f4004 Data : 0x0000000e
                 AW Phy Addr : 0x411f4004 Data : 0x00000000
    data 0
                 BW Phy Addr : 0x411f2004 Data : 0x00000001
                 AW Phy Addr : 0x411f2004 Data : 0x00000000
    data 1
                 BW Phy Addr : 0x41140084 Data : 0x00000001
                 AW Phy Addr : 0x41140084 Data : 0x00000001
    data 1
                 BW Phy Addr : 0x411a0084 Data : 0x00000001
                 AW Phy Addr : 0x411a0084 Data : 0x00000001
    data 1
                 BW Phy Addr : 0x41160034 Data : 0x00000001
                 AW Phy Addr : 0x41160034 Data : 0x00000001
    data 1
                 BW Phy Addr : 0x41121ff0 Data : 0x00000001
                 AW Phy Addr : 0x41121ff0 Data : 0x00000001
    data 1
                 BW Phy Addr : 0x41131fe4 Data : 0x00000000
                 AW Phy Addr : 0x41131fe4 Data : 0x00000001
    data 1
                 BW Phy Addr : 0x411e002c Data : 0x00000000
                 AW Phy Addr : 0x411e002c Data : 0x00000001
    data 1
                 BW Phy Addr : 0x481c52ec Data : 0x00000001
                 AW Phy Addr : 0x481c52ec Data : 0x00000001
    secss put in low power state
    data 1
                 BW Phy Addr : 0x48180900 Data : 0x00000001
                 AW Phy Addr : 0x48180900 Data : 0x00000001
    data 0
                 BW Phy Addr : 0x48180f00 Data : 0x00030000
                 AW Phy Addr : 0x48180f00 Data : 0x00030000
                 Phy Addr : 0x48180f10 Data : 0x00000000
    data 2
                 BW Phy Addr : 0x4818052c Data : 0x00000002
                 AW Phy Addr : 0x4818052c Data : 0x00000002
    data 2
                 BW Phy Addr : 0x48180508 Data : 0x00000302
                 AW Phy Addr : 0x48180508 Data : 0x00000302
    data 2
                 BW Phy Addr : 0x48180520 Data : 0x00000002
                 AW Phy Addr : 0x48180520 Data : 0x00000002
    data 2
                 BW Phy Addr : 0x48180524 Data : 0x00000002
                 AW Phy Addr : 0x48180524 Data : 0x00000002
    data 2
                 BW Phy Addr : 0x48180528 Data : 0x00000002
                 AW Phy Addr : 0x48180528 Data : 0x00000002
                 Phy Addr : 0x48180508 Data : 0x00000302
                 Phy Addr : 0x48180520 Data : 0x00000002
                 Phy Addr : 0x48180524 Data : 0x00000002
                 Phy Addr : 0x48180528 Data : 0x00000002
                 Phy Addr : 0x4c0000e4 Data : 0x00170209
    data 170209
                 BW Phy Addr : 0x4c0000e4 Data : 0x00170209
                 AW Phy Addr : 0x4c0000e4 Data : 0x00170209
                 Phy Addr : 0x4d0000e4 Data : 0x00170209
    data 170209
                 BW Phy Addr : 0x4d0000e4 Data : 0x00170209
                 AW Phy Addr : 0x4d0000e4 Data : 0x00170209
                 Phy Addr : 0x4c0000e4 Data : 0x00170209
    data 170209
                 BW Phy Addr : 0x4c0000e4 Data : 0x00170209
                 AW Phy Addr : 0x4c0000e4 Data : 0x00170209
                 Phy Addr : 0x4d0000e4 Data : 0x00170209
    data 170209
                 BW Phy Addr : 0x4d0000e4 Data : 0x00170209
                 AW Phy Addr : 0x4d0000e4 Data : 0x00170209
    DDR IOs RX is shutdown

     [host]  Setting L3 bandwidth regulator for [HDVICP0 ] to [press=[0,0] BW=900, WM Cycles=2500]

     [host]  Setting DMM priority for [HDVICP0 ] to [1] ( 0x4e000634 = 0x00000009 )
    Creat queue id:0
    queue id:0
    FileMngThread created
    Creat queue id:32769
    queue id:32769

     [host]  Setting DMM priority for [ISS     ] to [0] ( 0x4e000634 = 0x00800000 )
    AlramThread created
    Share memory init success
    IPNC_3.00.00 (swxx@itarge-desktop) (gcc version 4.3.3 (Sourcery G++ Lit
    Creat queue id:65538
    queue id:65538
    Creat queue id:98307
    queue id:98307
    queue id:32769

     [host] Attached to slave procId 2.


     [host] Attached to slave procId 1.
     [host] Attached to slave procId 0.

     [host] Loaded file ./firmware/ipnc_rdk_fw_m3vpss.xem3 on slave procId 2.
     [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
     [m3video] Remote Debug Shared Memory @ 0xbff05020
     [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040

     [host] Loaded file ./firmware/ipnc_rdk_fw_m3video.xem3 on slave procId 1.


     [host] Started slave procId 2.
     [host] Started slave procId 1.


     [host] After Ipc_loadcallback status [0x00000000]
     [host] After Ipc_loadcallback status [0x00000000]
     [m3video] ***** SYSTEM  : Frequency <ORG> - 200000000, <NEW> - 200000000
     [m3vpss ] ***** SYSTEM  : Frequency <ORG> - 200000000, <NEW> - 200000000
     [m3video] 
     [m3vpss ] notify_attach  rtnVal  0
     [m3video]  *** UTILS: CPU KHz = 400000 Khz ***
     [m3vpss ] initProxyServer  rtnVal  0
     [m3video] 
     [m3vpss ] 
     [m3video]  53: SYSTEM  : System Common Init in progress !!!
     [m3vpss ]  *** UTILS: CPU KHz = 400000 Khz ***
     [m3video]  53: SYSTEM: IPC init in progress !!!
     [m3vpss ] 
     [m3video]  53: SYSTEM: Attaching to [HOST] ...
     [m3vpss ]  95: SYSTEM  : System Common Init in progress !!!
     [m3vpss ]  96: SYSTEM: IPC init in progress !!!
     [m3vpss ]  96: SYSTEM: Attaching to [HOST] ...

     [host] Loaded file ./firmware/ipnc_rdk_fw_c6xdsp.xe674 on slave procId 0.

     [host] Started slave procId 0.

     [host] After Ipc_loadcallback status [0x00000000]

     [m3video]  1053: SYSTEM: Attaching to [HOST] ...
     [m3vpss ]  1096: SYSTEM: Attaching to [HOST] ...
     [m3video]  1096: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
     [m3video]  1096: SYSTEM: Attaching to [DSP] ...

     [host] After Ipc_startcallback status [0x097d2000]
     [m3vpss ]  1104: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
     [m3vpss ]  1104: SYSTEM: Attaching to [DSP] ...
     [host] After Ipc_startcallback status [0x097d2000]
     [m3video]  2096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  2104: SYSTEM: Attaching to [DSP] ...
     [m3video]  3096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  3104: SYSTEM: Attaching to [DSP] ...
     [m3video]  4096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  4104: SYSTEM: Attaching to [DSP] ...
     [m3video]  5096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  5104: SYSTEM: Attaching to [DSP] ...
    INIT: Entering runlevel: 5
     [m3video]  6096: SYSTEM: Attaching to [DSP] ...
     inside autorun
     [m3vpss ]  6104: SYSTEM: Attaching to [DSP] ...
     sbulla: unknown partition table
     sbulla: unknown partition table
    Starting system message bus:  [m3video]  7096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  7104: SYSTEM: Attaching to [DSP] ...
    dbus.
    Starting telnet daemonmkdosfs 2.11 (12 Mar 2005)
    unable to get drive geometry, using default 255/63/dev/sbulla has 255 heads and 63 sectors per track,
    logical sector size is 512,
    using 0xf8 media descriptor, with 1024 sectors;
    file system has 2 12-bit FATs and 4 sectors per cluster.
    FAT size is 1 sector, and provides 247 clusters.
    Root directory contains 512 slots.
    Volume ID is 4d81e90d, no volume label.
    .
    g_file_storage gadget: No serial-number string provided!
    g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
    g_file_storage gadget: Number of LUNs=1
    g_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/sbulla
     [m3video]  8096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  8104: SYSTEM: Attaching to [DSP] ...
    Starting syslogd/klogd: Simple mixer control 'PGA',0
      Capabilities: cvolume cswitch penum
      Capture channels: Front Left - Front Right
      Limits: Capture 0 - 119
      Front Left: Capture 80 [67%] [40.00dB] [on]
      Front Right: Capture 80 [67%] [40.00dB] [on]
    done

     _____                    _____           _         _  
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_| 
                  |___|                    |___|           

    Arago Project http://arago-project.org dm814x-evm ttyO0

    Arago 2010.11 dm814x-evm ttyO0

    dm814x-evm login: root (automatic login)
     [m3video]  9096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  9104: SYSTEM: Attaching to [DSP] ...
    queue id:0
     [m3video]  10096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  10104: SYSTEM: Attaching to [DSP] ...
    root@dm814x-evm:~# main 188
    ApproDrvInit: 3
    Creat queue id:131076
    queue id:131076
    main 192
     [m3video]  11096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  11104: SYSTEM: Attaching to [DSP] ...
    queue id:0
     [m3video]  12096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  12104: SYSTEM: Attaching to [DSP] ...
     [m3video]  13096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  13104: SYSTEM: Attaching to [DSP] ...
     [m3video]  14096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  14104: SYSTEM: Attaching to [DSP] ...
     [m3video]  15096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  15104: SYSTEM: Attaching to [DSP] ...
     [m3video]  16096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  16104: SYSTEM: Attaching to [DSP] ...
     [m3video]  17096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  17104: SYSTEM: Attaching to [DSP] ...
     [m3video]  18096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  18104: SYSTEM: Attaching to [DSP] ...
     [m3video]  19096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  19104: SYSTEM: Attaching to [DSP] ...
    TimeOut occure in boot_proc.
    Program exit.
     [m3video]  20096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  20104: SYSTEM: Attaching to [DSP] ...
     [m3video]  21096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  21104: SYSTEM: Attaching to [DSP] ...
    TimeOut occure in boot_proc.
    Program exit.
     [m3video]  22096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  22104: SYSTEM: Attaching to [DSP] ...
     [m3video]  23096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  23104: SYSTEM: Attaching to [DSP] ...
     [m3video]  24096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  24104: SYSTEM: Attaching to [DSP] ...
     [m3video]  25096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  25104: SYSTEM: Attaching to [DSP] ...
     [m3video]  26096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  26104: SYSTEM: Attaching to [DSP] ...
     [m3video]  27096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  27104: SYSTEM: Attaching to [DSP] ...
     [m3video]  28096: SYSTEM: Attaching to [DSP] ...
     [m3vpss ]  28104: SYSTEM: Attaching to [DSP] ...

     

  • 你好;

            你dsp的firmeware有加载成功吗? 看起来好像是dsp的firmeware 固件没有加载上

  • 是的,固件没有加载成功,但是为什么呢?

    这个系统现在跑在试验板上,与开发板的区别是我修改了其中的DDR芯片

    DDR芯片需要在dsp中重新初始化吗?感觉应该不需要。

    除了这个原因,还有什么可能的原因会导致dsp程序加载失败?

  • 你跟一下你加载 dsp 的 firmeware的位置,看程序执行了吗? 

    如果是dm385平台就不会加载dsp程序的,查一下这个位置看看

  • 如何跟踪这个过程呢?

    我的log信息里有:

     [host] Loaded file ./firmware/ipnc_rdk_fw_c6xdsp.xe674 on slave procId 0.

     [host] Started slave procId 0.

    我觉得这就是那个DSP程序的加载过程吧?

  • 嗯,这里是dsp程序的加载;

    如果dsp加载正常应对会有下面的打印

     [c6xdsp ]  
     [c6xdsp ]  *** UTILS: CPU KHz = 800000 Khz ***
     [c6xdsp ]  
     [c6xdsp ]  5: SYSTEM  : System Common Init in progress !!!
     [c6xdsp ]  5: SYSTEM: IPC init in progress !!!
     [c6xdsp ]  5: SYSTEM: Attaching to [HOST] ... 
     [c6xdsp ]  1029: SYSTEM: Attaching to [HOST] ... 
     [c6xdsp ]  1031: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
     [c6xdsp ]  1031: SYSTEM: Attaching to [VIDEO-M3] ...