This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

usb serial port ttyACM斷線問題



HI 各位大大 

    目前有一個問題 3G 網卡上網產生流量時例如觀看線上影片

    USB裝置會不定時斷線 也就是ttyACM會被Disconnect 在connect

    這時ttyACM0 就無法在下ATcommand 了 導致3G網卡就此斷線

    kernel 是3.2

    Android:4.2

    dmesg 訊息為

    

<3>[ 5978.217895] init: sys_prop: permission denied uid:1001 name:net.interfaces.defaultroute
<4>[ 6373.048767] jason---acm_tty_close
<4>[ 6373.052368] jason----tty_port_close_start
<4>[ 6390.900177] jason---acm_tty_close
<4>[ 6390.903839] jason----tty_port_close_start
<4>[ 6397.593231] jason---acm_tty_close
<4>[ 6397.597381] jason----tty_port_close_start
<4>[ 6397.601684] tty_port_close_start: tty->count = 1 port count = 0.
<4>[ 6397.825378] jason--1
<4>[ 6397.828704] jason---usb_disconnect
<6>[ 6397.832427] usb 1-1.1: USB disconnect, device number 3
<4>[ 6398.081665] jason--1
<6>[ 6398.403045] usb 1-1.1: new high-speed USB device number 4 using musb-hdrc
<6>[ 6398.531768] usb 1-1.1: New USB device found, idVendor=1546, idProduct=1102
<6>[ 6398.539062] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
<6>[ 6398.546722] usb 1-1.1: Product: u-blox Wireless Module
<6>[ 6398.552093] usb 1-1.1: Manufacturer: u-blox
<6>[ 6398.556488] usb 1-1.1: SerialNumber: 358901042067626
<3>[ 6398.587341] cdc_acm 1-1.1:1.0: This device cannot do calls on its own. It is not a modem.
<6>[ 6398.596527] cdc_acm 1-1.1:1.0: ttyACM0: USB ACM device
<3>[ 6398.627716] cdc_acm 1-1.1:1.2: This device cannot do calls on its own. It is not a modem.
<6>[ 6398.636871] cdc_acm 1-1.1:1.2: ttyACM1: USB ACM device
<3>[ 6398.646392] cdc_acm 1-1.1:1.4: This device cannot do calls on its own. It is not a modem.
<6>[ 6398.655578] cdc_acm 1-1.1:1.4: ttyACM2: USB ACM device
<3>[ 6398.671508] cdc_acm 1-1.1:1.6: This device cannot do calls on its own. It is not a modem.
<6>[ 6398.680816] cdc_acm 1-1.1:1.6: ttyACM3: USB ACM device
<3>[ 6398.690277] cdc_acm 1-1.1:1.8: This device cannot do calls on its own. It is not a modem.
<6>[ 6398.699493] cdc_acm 1-1.1:1.8: ttyACM4: USB ACM device
<3>[ 6398.721527] cdc_acm 1-1.1:1.10: This device cannot do calls on its own. It is not a modem.
<6>[ 6398.730926] cdc_acm 1-1.1:1.10: ttyACM5: USB ACM device
<3>[ 6398.740844] cdc_acm 1-1.1:1.12: This device cannot do calls on its own. It is not a modem.
<6>[ 6398.750244] cdc_acm 1-1.1:1.12: ttyACM6: USB ACM device

請各位大大 幫忙 謝謝

  • 从log上来说,USB设备已经被识别了,出现这种情况,建议你和3G 网卡的这个vendor联系一下,询问出现这个问题,是什么原因

    cdc_acm 1-1.1:1.0: This device cannot do calls on its own. It is not a modem.

  • HI Steven 

       恩 就上面LOG 看是已經被識別沒錯

       不過他是運作一段時間 被斷線  然後 又被認到

        認到之後 就無法使用

       我在想為何他會莫名被斷線   是不是因為 usb的 drivers 有bug  ??

       想請問一下 TI 的AM335X USB 軟體功能 是否有相關問題  


      謝謝