This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: AM623

Part Number: AM623


您好,我现在用到了最新的SDK:10_00_07_04,其中使用了EQEP和EPWM功能,需要完善下以后功能,麻烦你们能否协助开发一下。

1.EQEP需要支持CW/CCW模式,TRM文档里面是有此功能描述的,但是进行function的设置的时候是看不到的。

2.EQEP需要只是A/B正交1倍频模式,目前支持4倍频,文档里面有一些quadrature x1 的选项,但是无法设置成功。

3.EQEP功能能否自动计算出频率,方向等。

4.EPWM能否支持同一组EPWM使用时,具备有相位偏移的功能,也就是一组EPWM实现A/B正交输出功能。

5.EPWM功能能否支持设置脉冲个数,当脉冲计数到达之后自动关闭的功能。

谢谢!