请教几个问题:
1、PWMSS模块的时钟TBCLK是对系统时钟SYSCLKOUT进行分频得到的,资料上有5M、50M和250M的系统时钟输出(CM_PER_L4HS_CLKSTCTRL),对于PWMSS模块的SYSCLKOUT可以配置选择吗?
2、我的PWMSS0和PWMSS2模块可以正常使用,但是PWMSS1无法正常使用,对PWMSS1的寄存器进行映射后,读寄存器操作直接导致出错,初步判断应该是该模块未被激活,然后,当我想操作时钟电源管理模块的寄存器时也出现相同的错误(ioremap 0x44E00000地址成功,但是readl时就出现错误提示了)。错误:Unhandled fault: external abort on non-linefetch (0x1028) at 0xfa30221a 。如果是模块寄存器未被允许进行操作,请问PWMSS1和CM_PER的寄存器操作开关分别在哪儿啊?或者是有其他的什么原因也可以导致这样的问题