This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

raster例程的问题?



用的是C6748,starteware中例程raster,按照下面的步骤修改了,有光栅,无图像,查看缓存里面图像数据也有,请问应该怎么判断问题所在?以上是调试中的现象,谢谢了!

?In order to ensure LCDC bandwidth to prevent flicker issue, adjust system and LCDC configuration as below:
–1. set system configure register MSTPRIx to ensure LCDC is highest priority on SCR, other master lower than LCDC, 0 is highest priority.
–2. set DDR BPPBR register to 0x20 or less.
–3. set LCDDMA_CTRL[TH_FIFO_READY] = 5h or 4h, and
LCDDMA_CTRL[BURST_SIZE] = 4

–4. set RASTER_CTRL[PLM]= 2(data only) after LCD load palette.