This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: 16 Bit SPI

Part Number: TMS320C6748


您好,内存中有一段连续的数据需要用SPI发送给其他芯片,内存中的数据内容如下:

D0 D1 D2 D3 D4 D5 D6 D7
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18

发送顺序为从D0到D7,依次发送。

SPI配置为8Bit时,工作正常。

而配置为16Bit时,却是按D1、D0、D3、D2、D5、D4、D7、D6这样的顺序发送,即:先发送了高字节数据,然后再发低字节数据。

请问,有没有办法在配置为16Bit时,依然按照D0->D7这样的顺序发送?