TMS320C6713B通过BOOT程序烧录flash程序后,短时间内工作正常,重复上电也无异常;但断电放置一天后,IO等硬件工作正常(IO闪烁,串口也正常输出),但算法计算结果错误(重新烧录程序后算法正常输出)。开发平台为CCS V3.3
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320C6713B通过BOOT程序烧录flash程序后,短时间内工作正常,重复上电也无异常;但断电放置一天后,IO等硬件工作正常(IO闪烁,串口也正常输出),但算法计算结果错误(重新烧录程序后算法正常输出)。开发平台为CCS V3.3
您好
针对您描述的TMS320C6713B芯片在BOOT程序烧录flash程序后出现的问题,这里有几个可能的解决方向和检查点:
检查BOOT程序:
Flash芯片稳定性:
电源管理:
硬件连接与配置:
外部因素:
请从以上这些可能性核实您的目前情况以及遵从上述建议做对应的相关处理。