移植2014后出现该问题
U-Boot 2014.10 (Sep 07 2015 - 22:26:23)
Watchdog enabled I2C: ready DRAM: 512 MiB NAND: 1024 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - bad CRC, using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC cpsw, usb_ether Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Unable to read file boot.scr ** ** Unable to read file uEnv.txt ** ** No partition table - mmc 0 ** Card did not respond to voltage select! SD/MMC found on device 1 Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** Booting from nand ...
NAND read: incorrect device type in u-boot-spl-os
NAND read: incorrect device type in kernel Bad Linux ARM zImage magic!
怎办呢,请高手指教,我是菜鸟