This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM8127的uart口



求助

      在使用DM8127的uart2作为通讯口设计中,遇到uart2不能与外围设备通讯的问题,以下是设计原理:UART2_TX连接DM8127的U3引脚,UART2_RX连接DM8127的U4引脚;软件没有对内核驱动做修改;现象是:echo命令输出,无论使用ttyO0还是ttyO1、ttyO2、ttyO3、ttyO4、ttyO5都不能和外设通讯,示波器看也没有信号发出;另外,使用UART1_RX连接AF4,UART1_TX连接AG2是正常的;请问是什么原因导致?》是否是需要配置pincntl寄存器》?这个寄存器的bit0~bit7的pin multiplex对应表哪里可以找到?希望得到帮助!