This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM642 的VLIB使用



现在正在用DM642进行算法开发,准备使用ti提供的VLIB库(支持DM642的VLIB库的版本采用的是2.0和2.2)。
现在的问题是VLIB是不是只能在DSP/BIOS下使用?能不能在没有操作系统的工程中使用?
如果谁有EL_DM6437配套的VLIB实验手册的源码,能不能分享一下,感觉对这方面的学习会很有帮助的。
邮箱是xiaojienuaa@163.com。谢谢