This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6000问题请教



1、C6720的RESET引脚的纹波电压要求是什么,电流要求是否与其他IO引脚有区别。
 2、C6720的PLLHV就是PLL外部供电引脚纹波电压要求是什么,与普通IO口引脚是否有区别。
3、请发给我有关C6000程序优化的教程与例程下载链接,和CSR库和例程的下载链接。
4、是否可以超频1.5%