用于计算FFTC的数据放在L2RAM上运行时,是正常的,可以输出结果,但是将数据放在DDR3上时,FFTC就无法输出结果,使用ti例子进行测试的。这个跟FFTC本身有关吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用于计算FFTC的数据放在L2RAM上运行时,是正常的,可以输出结果,但是将数据放在DDR3上时,FFTC就无法输出结果,使用ti例子进行测试的。这个跟FFTC本身有关吗?
测试过L2和DDR3的情况,没有你说的情况,DDR3是否能够正常读写,FFTC的设置是否正确。
不会意思,之前说错了,不是FFTC的数据放在DDR3,是FFTC用到的描述符放在DDR3就跑不起来
这个也测试过,没有问题,你检查DDR3里的数据看有没有错误。
数据是没问题的,我是把堆栈设置到DDR3,Tool菜单下面的RTSC里面的stack memory也设置到DDR3,然后运行TI的例子工程,最后就在parseResult函数的时候无法接收到结果,错误码-6,。设置到L2SRAM是完全没问题的,并且将bcp的堆栈也设置到DDR3也都没问题。