This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

合众达提供的CCS4.1.2中编译自带的bios6项目程序时遇到的问题



我用的平台SEED-DTK6446,以及CCSV4,仿真器是XDS560plus。

具体问题是:

在CCS中新建了一个bios6的项目hello6,使用的CCSV4自带的hello例子程序,但是编译的时候一直有一个错误,不知是什么原因。

CCS中给出的错误提示如下:

<Linking>

fatal error: cannot open file

  "D:/Workspace/hello6_configuration/Default/configPkg/linker.cmd":

  Permission denied

>> Compilation failure

C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: *** [hello6.out] Error 1

C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors.

Build complete for project hello6

我看了一下D:/Workspace/hello6_configuration/,这个路径是所建立的工程的配置文件的路径,

其中D:/Workspace/hello6_configuration/Default/configPkg/linker.cmd这个文件不知为何打不开,我建立工程之后都从来没有去修改过这个文件,所以一直都编译不过去。

连CCSV4自带的例子程序都编译不了,这是CCS的问题吗?这问题困扰了我一段时间了,麻烦各位专业人士帮忙解决一下,谢谢了。