将C6713的工程移植到C6748上,工程是裸机程序。现在我有以下两个问题请教:
1.c6713可以正常处理的4ms中断,为什么在C6748需要更长的时间(改为8ms给一次中断信号)才能正常处理呢?????现在将 C6748的主频为400M,按说应该快的,怎么会比C6713慢呢?????
2.中断中主要是通过dsp的EMIFA和FPGA的数据交互,现在EMIFA的主频为100M,我想问一下EMIFA的最大主频是多少?是否可以通过提高EMIFA主频来提高交互速度呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
将C6713的工程移植到C6748上,工程是裸机程序。现在我有以下两个问题请教:
1.c6713可以正常处理的4ms中断,为什么在C6748需要更长的时间(改为8ms给一次中断信号)才能正常处理呢?????现在将 C6748的主频为400M,按说应该快的,怎么会比C6713慢呢?????
2.中断中主要是通过dsp的EMIFA和FPGA的数据交互,现在EMIFA的主频为100M,我想问一下EMIFA的最大主频是多少?是否可以通过提高EMIFA主频来提高交互速度呢?
将FPGA挂载在CS4上,时序配置如下:
setReg(EMIFA->CE4CFG,TA_MASK,3,TA_OFFSET);
setReg(EMIFA->CE4CFG,R_HOLD_MASK,3,R_HOLD_OFFSET);
setReg(EMIFA->CE4CFG,R_STROBE_MASK,20,R_STROBE_OFFSET);
setReg(EMIFA->CE4CFG,R_SETUP_MASK,1,R_SETUP_OFFSET);
setReg(EMIFA->CE4CFG,W_HOLD_MASK,1,W_HOLD_OFFSET);
setReg(EMIFA->CE4CFG,W_STROBE_MASK,6,W_STROBE_OFFSET);
setReg(EMIFA->CE4CFG,W_SETUP_MASK,2,W_SETUP_OFFSET);
setReg(EMIFA->CE4CFG,EW_MASK,0,EW_OFFSET);
setReg(EMIFA->CE4CFG,SS_MASK,0,SS_OFFSET);
应该怎么优化呢??????