This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

linux下使用DMtimer7的问题



各位大侠好 !

小弟在linux下使用DMtimer7每隔128ms产生一个中断,运行一段时候后发现周期由128ms变成了512ms 

代码如下:

//申请定时器7

p_timer = omap_dm_timer_request_specific(7);

//设置时钟源

src = clk_get(NULL, BB_32K_SOURCE);
if (IS_ERR(src))
return -EINVAL;
omap2_clk_enable(src);
__delay(300000);
omap2_clk_enable(p_timer->fclk);
__delay(300000);
omap2_clk_set_parent(p_timer->fclk, src);

if (IS_ERR_VALUE(res))
pr_warning("%s: timer%i cannot set source\n",
__func__, p_timer->id);

__delay(300000);
v = __raw_readl(p_timer->fclk->clksel_reg);
printk("the val of clksel_reg by omap2_clk_set_parent is %4x ####\n",v);

clk_put(p_timer->fclk);
clk_put(src);

请问各位有没有思路解决?谢谢