This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6422: Configure mode serial resistor selection

Part Number: AM6422

These resistor is used for boot mode config.

FAE suggest us increase the R to 1K and refer EVM or SK schematics. If not increased the R, failures that can happen.

We use a buffer AVC8T245 which has output impedance (as below photo shown)

We want to know the cause of the possible damage. If we don't change the resistors, what damages will happen? (high risk? or  low risk?)