This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

调用sendto函数不能主动发送给PC,只有PC发送给DSP后,DSP再调用sendto才可以发送到PC.



各位TI大神,请帮忙解答。

您好,我们原来的设计思路是6678有2个网口我们可以设置2个MAC,2个IP,这两个网口可以独立的和外部通信,但是我们发现无论2个MAC设置成什么,PC端收到的都是6678MACID寄存器的一个MAC.所以我们就把内部switch模块作为一个交换机,另外两个端口的MAC和IP是外边PC,这样实现了外部DSP两个网口都可以通信,但是有个问题,调用sendto函数不能主动发送给PC,只有PC发送给DSP后,DSP再调用sendto才可以发送到PC.