This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM67A: .wic sdcard boot problem

Part Number: AM67A

I use the following material

and tried countless permutation like

  • ubuntu22.04+balenaEtcher-1.19.25
  • windows11+balenaEtcher-Portable-1.18.11
  • windows11+balenaEtcher-1.19.21
  • windows10+balenaEtcher-Portable-1.18.11
  • windows10+balenaEtcher-1.19.21
  • windows11+balenaEtcher-1.19.25
  • windows11+rufus 4.5.2180
  • ...

to prepare booting sdcard.

But AM67A stuck at this step with sdcard booting

mnci: problen reading sD: status register

minc1: error -110 whilst initialising sD card

mmc1: problem reading sD: status register
minc1: error -110 whilst initialising sD card

mimc1: problem reading sD: Status register
.mmC1: .er.rOr..- 110: whilst initialising. .SD. cardmimc1: problem reading sD status register:ipc1: error -110 whilst initialisina sD card

need argent help

thx!