This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x开发板启动出现问题



开发板自带uboot可以正常启动,可是利用2014移植不行,打印如下信息,各位大神帮帮忙啊,万分感谢

U-Boot 2014.10 (Sep 17 2015 - 17:55:01)

       Watchdog enabled

 I2C:   ready DRAM:  512 MiB

 NAND:  1024 MiB

 MMC:   OMAP SD/MMC: 0,

OMAP SD/MMC: 1

Net:   cpsw,

 usb_ether Hit any key to stop autoboot:  0

NAND read: device 0 offset 0x280000, size 0x300000

  3145728 bytes read: OK

Wrong Image Format for bootm command

 ERROR: can't get kernel image! U-Boot#