This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6416TBGLZA8使用问题求助



您好,我们使用的是TMS320C6416TBGLZA8,采用外部晶振提供dsp的主时钟,晶振频率为40MHz,锁相环外部配置为20倍频。目前遇到的问题是,只要给锁相环供电,即PLLV pin提供3.3V电压,DSP的封装壳体上用频谱仪加开路线测试,就会发现在1.2G频率点出现一个很大的谐波,最大可能达到-60dBm。另外在1G附近,及1.5G附近也有谐波,目前这个问题影响到了我们系统的性能。

请教论坛内的各位专家以及ti的专家,帮忙分析一下这个问题,谐波通过何种手段才能去除掉?非常感谢