This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335Xuart1的四个管脚复用问题



现在我想将uart1的4个管脚作为gpio口使用终端接的继电器,在board-am335xevm.c中已经将uart1的初始化去掉,将4个管脚出事成io口如下

{"uart1_rxd.gpio0_14", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT}, /* 空闲 */
{"uart1_txd.gpio0_15", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT}, /* 空闲*/
{"uart1_ctsn.gpio0_12", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT}, /* 空闲 */
{"uart1_rtsn.gpio0_13", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT}, /* 空闲*/

也查找了在内核中也再无uart1的四个管脚的初始化操作,但是在内核启动期间,这四个口外界的蜂鸣器不停的间断响,知道再操作这几个端口时才能停止,不知道还有哪里对这几个端口进行了操作?请指教