This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.2 新建工程后不能使用头文件里预定义的变量类型或函数



IDE:CCS5.2

DSP:C5509A

问题:

之前一直在做仿真测试的时候,一直是导入已有的例程进行修改然后编译测试。今天想要自己建立一个工程,从头开始创建一个project,但是在include path设置正确的前提下,Source file里依然不能使用头文件里预定义的变量类型如Uint16,或者预定义的结构体如MCBSP_Config,或者函数如GPIO_FSET()。即使是把需要用的头文件放在project目录下,编译时依然会出现这些问题。我想请问,是不是CCS需要一些特别的设置?

谢谢,

Wayne