最近再调jpgenc ,用dvsdk2的demo可以用,但是我自己往codec server加的时候出现下面问题。
我的部分代码:
hEngine = Engine_open(envp->engineName, NULL, NULL);
printf("codec engine is %s\n", envp->engineName);
if (hEngine == NULL) {
ERR("Failed to open codec engine %s\n", envp->engineName);
cleanup(THREAD_FAILURE);
}
params.maxWidth = envp->imageWidth;
params.maxHeight = envp->imageHeight;
if (colorSpace == ColorSpace_YUV420PSEMI) {
params.forceChromaFormat = XDM_YUV_420SP;
} else {
params.forceChromaFormat = XDM_YUV_422ILE;
}
dynParams.inputChromaFormat=XDM_YUV_420SP;
dynParams.inputWidth = params.maxWidth;
dynParams.inputHeight = params.maxHeight;
hIe = Ienc1_create(hEngine, envp->videoEncoder, ¶ms, &dynParams);
调试信息如下:
Algorithm creation FAILED; make sure that 1) alg params are correct/appropriate,
2) there is enough internal and external algorithm memory available -- check DSKT2 settings for heap assignments and scratch allocation @1,055,065us: [+0 T:0x49d8d490] ti.sdo.ce.alg.Algorithm - Algorithm_delete> Enter(alg=0x138fe98)
@1,055,264us: [+0 T:0x49d8d490] ti.sdo.ce.alg.Algorithm - Algorithm_delete> Exit
@1,055,410us: [+0 T:0x49d8d490] ti.sdo.ce.alg.Algorithm - Algorithm_create> return (0x0)
@1,055,548us: [+2 T:0x49d8d490] CV - VISA_create2> FAILED to create local codec.
@1,055,864us: [+0 T:0x49d8d490] CV - VISA_delete(0x11a43d8)
@1,056,280us: [+5 T:0x49d8d490] CV - VISA_delete> deleting codec (localQueue=0xffff, remoteQueue=0xffff)
@1,056,504us: [+0 T:0x49d8d490] ti.sdo.ce.image1.IMGENC1 - IMGENC_create> return (0x0)
@1,058,105us: [+7 T:0x49d8d490] ti.sdo.dmai - [Ienc1] Can't open imaging encode algorithm
Error: Failed to create video encoder: jpegenc
急求ti的大师怎么解决?谢了。